{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Video: Increasing ATV21 & ATV212 High Speed Setting Beyond 60Hz.

Article available in these languages: Finnish

Issue:
ATV212 and ATV12 High Speed Setting Beyond 60Hz.

Product Line:
ATV21 ATV212 S-Flex

Environment:
All serial numbers

Cause:
Overspeed operation is desired.

Resolution:
First, set the maximum frequency, FH, to at least the desired high speed.
Second, change the upper limit, UL, to the desired high speed.

If an analog input is used for speed reference, it will need to be scaled:
If FMOd=1, VIA analog input, then set F204 to the high speed.
If FMOd=2, VIB analog input, then set F213 to the high speed.