{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the ATS22 adjustable range for ILt, current limit?
Issue:
Current Limit range for ILT on ATS22.

Product Line:
ATS22

Environment:
All models

Cause:
N/A

Resolution:

Set the motor current limit applied during the soft start.
With at maximum load, the ILT should be set to a high enough value to allow motor start.  The range is 200% to 700% of parameter In, motor rated current. The maximum is limited to 350% of the ATS22 amp rating.
If the application requires more than 350% of the ATS22 rating, then the soft starter must be upsized.


Schneider Electric Global