Issue:
Use start/stop on LI1 and set a LSP speed on ATV312 drive.
Use start/stop on LI1 and set a LSP speed on ATV312 drive.
Product Line:
ATV31 and ATV312
Environment:
All models and serial numbers
Cause:
None
All models and serial numbers
Cause:
None
Resolution:
Enter the motor parameters in the DRC menu (BFR: UNS, FRS: NCR: NSP).
Wire a start/stop contact between LI1 and +24V. Set low speed in the SET menu with parameter LSP. Assign the value in frequency.
Enter the motor parameters in the DRC menu (BFR: UNS, FRS: NCR: NSP).
Wire a start/stop contact between LI1 and +24V. Set low speed in the SET menu with parameter LSP. Assign the value in frequency.
Released for:Schneider Electric Global