{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
On a new S-Flex installation, why does the motor run correctly in bypass and incorrectly in AFC?

Issue:
The motor runs forward in bypass but reverse in AFC.

Product Line:
S-Flex

Environment:
S-Flex with BYPASS feature

Cause:
None

Resolution:
In BYPASS mode, the power supply phase rotation passes straight through to the motor.  In AFC mode, the VFD chops the AC power to DC and then creates an independent phase rotation on the Pulse Width Modulation output to the motor.  Therefore, a new installation can initially result in various combinations of forward/reverse motor rotation in BYP/AFC modes.  The Instruction Bulletin provides the preferred method to correct the motor rotation in both BYP and AFC modes.  See the attached file.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Global

Attachment(s)
S-Flex212 motor rotation.pdf [79 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.