Issue:
mA signal configuration on the ATV312 Drive
Product line:
Altivar ATV312
Environment:
All models, all serial numbers
Cause:
This drive uses terminals AI3 and COM for the mA signal. It can be configured as 0-20mA or 4-20mA.
Resolution:
Under the I-O_ menu go to CRL3 to adjust the minimum value and CRLH to adjust the maximum value.
mA signal configuration on the ATV312 Drive
Product line:
Altivar ATV312
Environment:
All models, all serial numbers
Cause:
This drive uses terminals AI3 and COM for the mA signal. It can be configured as 0-20mA or 4-20mA.
Resolution:
Under the I-O_ menu go to CRL3 to adjust the minimum value and CRLH to adjust the maximum value.
Released for:Schneider Electric Global