What communication protocols are available for the ATV61 and ATV71?
Published date:
25 November 2019
Issue:
Communication protocols available on the ATV61 and ATV71 drives
Product Line:
Altivar 71, Altivar 61
Environment:
All models, All serial numbers
Cause:
Network options for the ATV61 and ATV71 drives
Resolution:
The Altivar 61 and Altivar 71 series Variable Frequency Drives are equipped with Canopen and Modbus RTU from the factory. Other options are available as follows:
The new BACnet option card (VW3A3319) is equipped with a 4 position, removable connector in place of the female sub D 9 pin connector on the old option card. This change has been requested by the market place and will make network connections easier, allow installers to daisy chain network wiring and reduce installation time.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.