Issue:
ATV21 / ATV212 drive has a flashing C on the screen
Product Line:
Altivar 21, Altivar 212.
Environment:
All models, All Serial numbers.
Cause:
Motor current in excess of the value set in F601. Note: If F701 is set to 1, then F601 setting is in Amperes. If parameter F701 is set to 0 then F601 setting is in percentage of the drive rated output current as listed on the drive nameplate. Factory default for F701 is 1, to indicate Amperes.
Resolution:
Ensure that F701 [Unit value selection (either % or Amps / Volts)] is set to desired setting, and:
F601 is set properly for the motor being used:
If these settings are correct, and current limit is still being reached, adjust the acceleration time (ACC) to a higher value.
If Current limit is still being reached, investigate the incoming voltage to the drive:
If the incoming voltage is dropping significantly when the run command is given, then the motor will naturally pull more current.
“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Released for:Schneider Electric Global