{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is the remote graphic keypad display, VW3A1101, compatible with the ATV312 drive?
Issue:
Can you use VW3A1101 with ATV312 drive?

Product Line:
ATV312

Environment:
All models

Cause:
Display

Resolution:
Yes, the VW3A1101 keypad is compatible with the ATV312 drive.  The keypad must have minimum CPU V1.2IE09.

It is not direct connected to the drive.  At minimum, an adaptor and a cable are required:
VW3A1105 is a female-female adaptor between cable and keypad
VW3A1104R10 is a 1meter cable
VW3A1104R30 is a 3meter cable
VW3A1104R50 is a 5meter cable
VW3A1104R100 is a 10meter cable

An optional remote mount kit, VW3A1102, will include the VW3A1105 adaptor.
An optional door, VW3A1103, adds to the remote mount kit to increase IP54 rating to IP65.

Schneider Electric Global