{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Smart-UPS VT-Galaxy 3500; Run time below limit, run time threshold alarms

Article available in these languages: Spanish

Issue:
Smart-UPS VT-Galaxy 3500; Run time below limit, run time threshold alarms
Product line:
Smart-UPS VT-Galaxy 3500
Environment:
All models, all serial numbers
Cause:
Run time below limit, run time threshold alarms may be seen if the user settable threshold is surpassed. This setting may be adjusted per the customer’s requirements.
Resolution:
Adjust the run time alarm threshold in the display or replace batteries

Display menu; Setup>Alarms>Alarm Thresholds>Run Time

Schneider Electric Global