Issue:
Will the CX fit through a standard door opening?
Product Line:
NetShelter CX
Environment:
All versions and serial ranges.
Cause:
Need to ensure the NetShelter CX will fit up the stairs, into the elevator or through a doorway.
Resolution:
All the units, including the 38U, are designed to go through a standard doorway. They measure 750 mm /29.5” wide x max 1950mm/76.7” tall.
Will the CX fit through a standard door opening?
Product Line:
NetShelter CX
Environment:
All versions and serial ranges.
Cause:
Need to ensure the NetShelter CX will fit up the stairs, into the elevator or through a doorway.
Resolution:
All the units, including the 38U, are designed to go through a standard doorway. They measure 750 mm /29.5” wide x max 1950mm/76.7” tall.
Released for:Schneider Electric Global