Issue:
Needs a Power board for ATV71HC11N4
Product line:
ATV71 and ATV61
Environment:
All models, all serial numbers
Cause:
Power board not functional
Resolution:
The Power board for these drive is VX5A1HC1113.
It is required to check the Serial number of the drive before ordering the Power Board.
If the 8th digit in the serial number is 2, the drive was built using Fuji IGBT's instead of the standard Mitsubishi IGBT's. A drive with Fuji IGBT's requires a modified version of the Power board (VX5A1HC1113F). IGBT, and gate driver board parts also will have an F at the end.
Needs a Power board for ATV71HC11N4
Product line:
ATV71 and ATV61
Environment:
All models, all serial numbers
Cause:
Power board not functional
Resolution:
The Power board for these drive is VX5A1HC1113.
It is required to check the Serial number of the drive before ordering the Power Board.
If the 8th digit in the serial number is 2, the drive was built using Fuji IGBT's instead of the standard Mitsubishi IGBT's. A drive with Fuji IGBT's requires a modified version of the Power board (VX5A1HC1113F). IGBT, and gate driver board parts also will have an F at the end.
Released for:Schneider Electric Global