Issue:
Programming forward and reverse on the ATV61 and ATV71
Product Line:
ATV61 ATV71
Environment:
All ATV61 and 71 drives
Resolution:
For the ATV71:
Programming forward and reverse on the ATV61 and ATV71
Product Line:
ATV61 ATV71
Environment:
All ATV61 and 71 drives
Resolution:
For the ATV71:
- When in 2 wire control: LI1 is forward and LI2 is the Reverse command.
- When in 3 wire control: LI1 is the Stop input, LI2 is the Forward Command and LI3 is the Reverse Command
- In Menu 1.5 [Inputs/Outputs CFG] the
rrsS
[Reverse Assign] parameter can be assigned to other unused logic inputs.
- When in 2 wire control: LI1 is Forward Command and Reverse Assign is set to NO.
- When in 3 wire control: LI1 is Stop, LI2 is Forward and Reverse Assign is set to NO.
- In Menu 1.5 [Inputs/Outputs CFG] the rrsS [Reverse Assign] parameter can be assigned to any unused logic input.
Released for:Schneider Electric Global