{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Does ATV32 drive have Brake Logic control?
Issue:
Is Brake Logic Control Avilable in the ATV32 Drive?

Product line:
Altivar 32, ATV32

Environment:
All models, all serial numbers

Cause:
NA

Resolution:
ATV32 drive does have Brake Logic Control function parameters.
Refer to the ATV32 Programming manual, ATV32_programming_manual_S1A28692_01

Schneider Electric Global