Issue:
How is an ATS48 set up for basic programming?
Product line:
Altistart 48
Environment:
All models, all serial numbers
Cause:
Basic programming set up for the ATS48 soft starters.
Resolution:
SET menu:
IN= FLA motor amps
ACC= acceleration
STY= type of stop (f=freewheel, d=ramp stop, b=intel braking)
DEC= deceleration [only appears if Sty= d (ramp stop)]
ILT=current limit 400% or 4X your motor current is default value.
DRC menu:
CLP= Off (Torque Control). This is important if the ACC/DEC times have to be followed exactly.
Refer to the ATS48 User Manual for any further details.
The following video demonstrates this initial setup procedure:
How is an ATS48 set up for basic programming?
Product line:
Altistart 48
Environment:
All models, all serial numbers
Cause:
Basic programming set up for the ATS48 soft starters.
Resolution:
SET menu:
IN= FLA motor amps
ACC= acceleration
STY= type of stop (f=freewheel, d=ramp stop, b=intel braking)
DEC= deceleration [only appears if Sty= d (ramp stop)]
ILT=current limit 400% or 4X your motor current is default value.
DRC menu:
CLP= Off (Torque Control). This is important if the ACC/DEC times have to be followed exactly.
Refer to the ATS48 User Manual for any further details.
The following video demonstrates this initial setup procedure:
Released for:Schneider Electric Global