{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Which Altistart soft starters are available with 24Vdc logic inputs?

Article available in these languages: Spanish

Issue:
Altistarts with 24Vdc logic inputs.

Product line:
Altistart ATS Softstarts

Environment:
ATS48 ATS01 ATS22

Cause:
Requires 24Vdc logic inputs.

Resolution:

The following product lines use 24Vdc logic inputs
  • ATS48: all models
  • ATSU01 all models
  • ATS01 models with suffix LU / QN / RT / FT (not Q / LY)
  • ATS22 models with suffix S6 (not S6U)