Check the Line voltage power, input connections and or fuses.
Check to see if you are single phasing the input on the drive.
Reset the drive.
Disable the detection by setting input phase loss to "No." (IPL parameter is found in the FLt menu and can be changed if the drive is not running) Then run and check current on each phase to be sure it is balanced (for 3 phase power).
If single phase input voltage, set IPL to NO
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.