Issue:
is there a maximum distance of the cables connected between the drive and motor?
Product Line:
Altivar ATV61 and ATV71
Environment:
All
Cause:
Application notes on motor cable distance.
Resolution:
Length of motor cables from ATV71
Released for:Schneider Electric Global