{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Does the ATV61 Drive need to have a motor connected to perform diagnostic tests?
Issue:
ATV61 diagnostic tests conditions

Product Line:
Altivar 61, Altivar 71

Environment:
All models, All serial numbers.

Cause:
Would like to perform thyristor and transistor tests on the drive.

Resolution:
A motor must be connected to the output of the drive in order to perform the transistor self diagnostic tests.