{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the conduit kit for an ATV61 or ATV71 for frame size 9?

Issue:
Part number for an ATV61HD90N4 or frame size 9 conduit kit.

Product Line:
ATV61, ATV71

Environment:
ATV61HD55M3X, ATV61HD75M3X,  ATV61HD90N4, ATV61HC11N4
ATV71HD55M3X,  ATV71HD90N4

Cause:
Mounting requirements.

Resolution:
VW3A9209 is the NEMA Type 1  Conduit Kit.  It includes a metal box with conduit knockouts.  This accessory provides a NEMA 1 enclosure rating for the drive and provides a surface area to land conduit when wall mounting the drive.

Schneider Electric Global