{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

What is the Serial Number to use when installing SFT2841?

Article available in these languages: Czech

Product Line
SEPAM Relays
SFT2841

Environment
SEPAM SFT2841 software installation

Resolution
The serial numbers to use while installing the software are:
- For SFT2841 versions 11 and above: 0647740-08
- For SFT2841 versions below 11: 8888888-06

Did this answer your question?

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.