{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What type of temperature APS_SENSORS may be connected to Sepam 1000+?


For more accurate protection of transformers and motors against overload situations, Sepam 1000+ is able to measure eight temperatures.

Three different types of temperature APS_SENSORS can be connected to the eight temperature inputs on the optional module of Sepam 1000+. These types are Pt100, Ni100 and Ni120.

Re-published to revised security level: 18 June 2008 by DRM

Applies To: Sepam 1000+ (Sepam Series 20 and Sepam Series 40)

Public

All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL166640 V2.0, Originally authored by LaVI on 06/20/2008, Last Edited by DaMi on 06/20/2008
Related ranges: Sepam series 20, Sepam series 40

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.