Effects of interruptions of the DC power supply. (CEI60255-11)
The effects are determined for an interruption with a duration chosen in the following list and declared by the manufacturer : 2 _ 5 _10 _ 20 _ 50 _ 100 _ 200 ms
The interruption must be sudden, i.e. the auxiliary power supply must vary from 0 to the rated value and the opposite .
The relay must not change erroneously its output status when the power supply value is applied or cancelled.
Fugitive cancelling Sepam 1000+ S20: 10ms.
Fugitive cancelling Sepam 1000+ S40: 20ms.
Fugitive cancelling Sepam Series 80: 100ms
Released for:Schneider Electric Global