{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can you perform voltage protection with a SEPAM Series 20?

Yes, please refer to the SEPAM Series 20 Selection Table in the reference manual for more detail on which protection functions are available on Series 20 devices.

Original article#3617
Re-published to revised security level: 17 June 2008 by DRM

Applies To: Sepam 20

Public

All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL184475 V2.0, Originally authored by DaMi on 06/15/2007, Last Edited by DaMi on 06/18/2008
Related ranges: Sepam series 20

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.