{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How many samples per cycle are captured for the Sepam Series 20, 40,60 and 80?

Issue
What is the resolution of the waveform captures for the Sepam relay?

Product Line
Sepam 20 Series
Sepam 40 Series
Sepam 60 Series
Sepam 80 Series

Resolution
The Sepam protection relay samples at 36 samples per cycle to calculate true RMS values for displayed phase current and overload protection. It can analyzes up to the 17th harmonic. All other measurements and protection values are calculated from the fundamental RMS calculation. The fault recording displays (waveform capture) only 12 samples per cycle for the Series 20 and 40. The Series 80 relay has an additional option of choosing 36 samples per cycle. Fault recording can be configured using SFT2841:
Image 1

Schneider Electric Global