{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the ACE917?

Product Line
LPCT
ACE917

Environment
Testing

Resolution
The ACE917 is an adapter that is used to test the protection chain using as standard injection box, when the SEPAM relay is connected to LPCT APS_SENSORS.
Attached is the manual for the ACE917

Schneider Electric Global

Attachment(s)
LPCT type current sensors.pdf [182.81 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.