Issue:
What are some concerns to be aware of when connecting a generator to a ATS48 soft start?
Product Line:
ATS48
Environment:
Generator
Cause:
n/a
Resolution:
Main constraint: the generator must deliver the starting current with the minimum variation of the voltage frequency and drop voltage, in all cases within the tolerances written in the catalog.
So, the power of the generators depends on the acceleration ramp and the current limitation set in the ATS48.
Once the motor is working at its nominal power, the generator delivers the nominal current of the motor.
Generally, 2 times the motor power is enough.
The generator power can be decreased (optimized) if the cycles of the application are well known and if it's sure it will not change in the future.
Legacy KB System (APS) Data: RESL159916 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altistart 48
Released for: Schneider Electric Global