Issue:
ATV31 : Remote terminal VW3A31101, LCC in CtL menu, how to do a run reverse command/order with keypad?
Product Line:
Altivar ATV31
Environment:
All serial numbers, all model numbers.
Cause:
Customer can't do a run reverse with deported keypad, but can do the run forward
Resolution:
By default, the only authorized direction is forward.
To be able to run also in reverse direction, the parameter ROT (in Ctl menu ) must be Set to the value "Bot" (for both directions)
Note : The parameter ROT appears in Ctl menu ONLY if the control is taken by LCC.
Released for:Schneider Electric Global