Issue: ATV31 - ATV71 overvoltage threshold OSF.
Product Line: ATV31 ATV71
Environment: ATV71***N4 ATV31***N4
Cause: Overvoltage threshold
Resolution:
Description: Line voltage too high
OSF : overvoltage when the drive is not running
OSF Fault cannot be automatically reset. The cause of the fault must be corrected before resetting by cycling the power:
ATV71 OSF Thresholds:
200V Range 400V range
OSF high 269Vac 535Vac
OSF low 265Vac 530Vac
ATV31 OSF Thresholds:
200V Range 400V range 500V range
OSF high 283Vac 594Va 707Vac
OSF low 268Vac 560Vac 670Vac
Legacy KB System (APS) Data: RESL173050 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 71
Released for:Schneider Electric Global