Issue:
Vijeo Designer simulation running time
Product Line:
Vijeo Designer
Environment:
HMI Configuration Software
Resolution:
The simulation build in Vijeo Designer V6.2 runs for up to 1 hours.
It must be restarted to get another hour..
To run longer time a Vijeo Designer Runtime license is required. The part number for the Runtime license are as follow:
VJDSNRTMPC --Vijeo Designer Runtime Magelis iPC for Runtime version 6.2 SP10 and below
VJDSNRTSPC ---Vijeo Designer Runtime Standard PC for Runtime version 6.2 SP10 and below
The 4 new part numbers for Vijeo Designer V6.2 SP11 and above Runtime are as follows:
1) VJDRPCCZLSPMZZ – Vijeo Designer Runtime Standard PC – Printed
2) VJDRPCCZLSPAZZ - Vijeo Designer Runtime Standard PC – Emailed
Licenses 1 and 2 support:
Generic PC
Harmony P6
Harmony iPC except box PC HMIBMP
Harmony iPC except box PC HMIBMU
Harmony iPC except panel PC HMIPSO
Harmony iPC except panel PC HMIPSP
Harmony iPC except panel PC HMIPEP
3) VJDHPCCZLSPMZZ – Vijeo Designer Runtime Harmony PC - Printed
4) VJDHPCCZLSPAZZ - Vijeo Designer Runtime Harmony PC - Emailed
Licenses 3 and 4 support:
Harmony iPC box PC HMIBMP
Harmony iPC box PC HMIBMU
Harmony iPC panel PC HMIPSO
Harmony iPC panel PC HMIPSP
Harmony iPC panel PC HMIPEP
Released for:Schneider Electric Global