{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What Schneider devices will connect using the (TCSMCNAM3M002P) USB to RS485 converter?


The TCSMCNAM3M002P is compatible with the following device families (RJ45 socket):

Advantys OTB
Altistart Series
Altivar series incl. HMI
Altivar Controller inside,
SD3 28 Stepper Drive
Lexium Motion Controller
Lexium Servo Drives
Magelis XBT N/R/RT
M238 and M340 Controller,
TesysU / TesysT System
XPS MC Safety Controller

Note: TCSMCNAM3M002P is NOT compatible with Modicon Quantum and Modicon Momentum. Due to a different connector pinout.


Legacy KB System (APS) Data: RESL201395 V1.0, Originally authored by GeMc on 02/19/2010, Last Edited by GeMc on 02/19/2010
Related ranges: Magelis XBT N, R, RT, Modicon M340