Goals and Symptoms
EDS-file for Lexium 17D to import into the Unity Pro Hardware catalogue does not work.
Causes and Fixes
Please find in the attachment the modified eds-file.
The Problem was in the default mapping, there was one object mapped several times in one PDO. The default mapping is changed now and it works also in Unity 4.0/4.1 as well.
Modified eds for the Lexium 17:
Attachments
(Removed File URL: 199945_CB26/Lexium17D_mod.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/04b1bdb58c577464c12576320052aa54/fl_block_5/0.620?OpenElement&FieldElemFormat=gif)(Removed File URL: 199945_CB26/HardwareCatalogManager.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/04b1bdb58c577464c12576320052aa54/fl_block_5/0.143E?OpenElement&FieldElemFormat=gif)
Legacy KB System (APS) Data: RESL199945 V1.0, Originally authored by MaPr on 09/15/2009, Last Edited by MaPr on 09/15/2009
Related ranges: Lexium 17D
Released for:Schneider Electric Global