{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How can we use EnDat 2.1 on LXM32-M?

Goals and Symptoms

How can we use EnDat 2.1 on LXM32-M?

Facts and Changes

In the catalogue, it says that EnDat 2.1 can be used for both machine and motor encoder, but in the encoder manual , we found no information for this. And in the parameter ENC2_type , we can not find endat 2.1 to choose.

Causes and Fixes

The information in the catalogue are wrong. With LXM32 it is not possible to use an EnDat 2.1, it¿s only possible to use an EnDat 2.2 but not for a motor encoder it¿s only possible to use it for a machine encoder.
In the attachment you can find a list with the supported interfaces.

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.