{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Which firmware version of ILA2E and ILA2E supports the synchronous operation mode for using in TwinCAT-NC?

Goals and Symptoms

Which firmware version of ILA2E and ILA2E supports the synchronous operation mode for using in TwinCAT-NC?

Causes and Fixes

ILA2E and ILE2E supports the synchronous operation mode from firmware version >=V1.015 (>=RS01).
If the device identification plate shows a lower version, the synchronous operation mode are not supported and cannot be updated !!!

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.