This table reflects the mean time between failures in hours for each of the older ConneXium PRODUCTS. If you divide the total hours by 8760 (number of hours in a year), you will get the total number of years between failures. If you divide 720 (hours in a month) you will have the total months between failures.
ConneXium
Part Number | Description | MTBF in Hours |
499NEH00410 | DIN Rail 10Base-TP Hub (4 10Base-T RJ45 Ports) | 1,399,091 |
499NEH04100 | DIN Rail 100Base-TX Hub (4 100Base-TX RJ45 Ports) | 1,182,145 |
499NEH00510 | DIN Rail 10Base-TP/FL Hub (3 10BaseT RJ45, 2 10BaseFL ST Multimode Ports) | 347,000 |
499NOS07100 | DIN Rail 10/100 Base-TX/FX Switch (5 10/100 RJ45, 2 Redundant Duplex SC Multimode Ports) | 171,000 |
499NES07100 | DIN Rail 10/100 Base-TX/TX Switch (5 10/100 RJ45, 2 Redundant RJ45 Ports) | 177,000 |
499NES08100 | DIN Rail 10/100Base-TX Switch (8 10/100Base-TX RJ45 Ports) | 454,000 |
499NTR00010 | DIN Rail 10Base-TP/FL Transceiver, Multimode | 1,196,387 |
499NTR00100 | DIN Rail 100Base-TX/FX Transceiver, Multimode | 1,200,523 |
Legacy KB System (APS) Data: RESL120001 V2.0, Originally authored by on , Last Edited by on
Related ranges: ConneXium - Ethernet
Released for:Schneider Electric Global