Issue
Do you need to use RIO taps on a network that consists only of a primary rack and one remote rack?
Product Line
Other network, fieldbus, protocols
Environment
Quantum RIO
Resolution
Yes, taps must be used to provide proper attenuation of the signal and proper isolation of the drop from the trunk cable.
Released for:Schneider Electric Global