Issue:
Does the Advantys bus termination plate STBXMP1100 come with the NIM module or does it have to be ordered separately?
Product Line:
Advantys
Environment:
Advantys Configuration Software
Cause:
Customer not sure if they lost the termination plate and if it comes with it or if it has to be ordered separately.
Resolution:
The Advantys bus termination plate does not have to be ordered separately. The bus termination plate is shipped with each NIM module, however, a replacement bus termination plate can be ordered as part number: STBXMP1100.
Released for:Schneider Electric Global