Goals and Symptoms
What is the maximum current draw (amps) at CL1 and CL2 at 115VAC for each ATS48 model?
Facts and Changes
ATS48 CL1 and CL2 power with cooling fans working
Causes and Fixes
For each card without fan under 115 Vac: 220 mA
With fans:
D32 to C17 : 260 mA
C21 to C32 : 440 mA
C41 to M12 : 700 mA
Legacy KB System (APS) Data: RESL160577 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altistart 48
Released for:Schneider Electric Global