{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How do I read or write a program to/from the SY/MAX model 50 controller to the 8005PR4 hand held programmer?

Issue

How do you I read or write a program to/from SY/MAX model 50 controller to the 8005PR4 hand held programmer?

Product Line

SY/MAX

Environment

80005PR4

Resolution

To read a program from the SY/MAX model 50 controller to the 8005PR4 enter the following sequence:

  1. TRS, READ.
  2. Once "TRS P T L GO?" is displayed make sure the CPU is halted and a memory pack is installed and then press the ENTR key. "TRS P T L" is displayed during execution.
  3. When completed "TRS P T L END" is displayed.


To write a program from the 8005PR4 to the SY/MAX model 50 controller enter the following sequence:

  1. TRS, ENTR.
  2. Once "TRS L T P GO?" is displayed make sure the CPU is halted and either a 8005MP1 or 8005MP4 CMOS RAM memory pack is installed and then press the ENTR key. "TRS L T P" is displayed during execution.
  3. When completed "TRS L T P END" is displayed.