Issue
Why don't I have the option for TCP/IP in the ProWorx NxT Configuration Extension for the Quantum 140CPU11302 and the 140CPU11303 controllers?
Product Line
Quantum, ProWorx NxT
Environment
ProWorx NxT, 140CPU11302
Resolution
The problem is the wrong REV controller has been selected. The TCP/IP option is only available for the Quantum 140CPU11302 and 140CPU11303 REV 2 controllers. The TCP/IP option is not available for the REV 1 controllers in the NxT Add Configuration Extension window.
Released for:Schneider Electric Global