Issue
Can a Unity Quantum project be converted to a Unity Premium project?
Product Line
Unity Pro, Quantum, Premium
Environment
Unity Pro v8.0
Resolution
No, the two product lines support different IO and different instruction sets. This type of conversion is not available. Converting a Unity Premium project to a Unity Quantum project is also not possible for this reason.
The Schneider Electric recommendation is to upgrade for a M580 controller using the Unity to M580 Converstion (UMAC) tool.
Released for: Schneider Electric Global