{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Are there any simulator modules available for the Quantum series?

Issue

Are there any simulator available for the Quantum series?

Product Line

Modicon Quantum

Environment

140XSM0100

Resolution

There are two types of simulator modules available for the Quantum series.
The 140XSM00200 discrete simulator module consists of 16 toggle switches which are used to generate up to 16 binary input signals.
The 140XSM01000 analog simulator module is used for simulating 4-20mA field current loops used with current input Quantum modules.