{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What are the physical dimension specifications for the single slot Quantum modules?

Issue
What are the physical dimension specifications for the single slot Quantum modules?

Product line
Modicon Quantum

Environment
140CPU67261

Resolution
The dimensions for the single slot Quantum modules are:
Height = 9.84 in. (250 mm)
Depth = 4.09 in. (103.85 mm)
Width = 1.59 in. (40.34 mm)

Schneider Electric Global