Issue
What is the difference between the Quantum 140CRP93100 and 140CRP93200 Remote I/O modules?
Product line
Modicon Quantum
Environment
140CRP93100
Resolution
The main physical difference is the external connection. The 140CRP93100 has only one channel. The 140CRP93200 has two channels. The following chart lists the specification differences:
140CRP93100 | 140CRP93200 | |
Bus Current Required | 600 mA | 750 mA |
Power Dissipation | 3 W | 3.8 W |
Released for:Schneider Electric Global