{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
STB Island Module Hot-Swapping Information

Issue

The purpose of this resolution is to inform STB users of a point regarding hot swapping the islands I/O modules.

Product Line
Advantys,STB

Resolution

STB design does not allow hot-swapping of an I/O module if there is only one module in the island. The same is true if you have multiple modules and you remove all of them prior to replacing one. The NIM will enter fatal error and require a power cycle to resume operation once the module is replaced.


Legacy KB System (APS) Data: RESL176389 V1.0, Originally authored by on , Last Edited by on
Related ranges: Advantys STB

Schneider Electric Global