{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Conversion of a Modsoft program to a Proworx 32 project fails.

Goals and Symptoms

Conversion of a Modsoft program to a Proworx 32 project fails.

Facts and Changes

ProWORX 32 version 2.0

Causes and Fixes

Converting a Modsoft program to 'ProWORX 32' could sometimes fail and return errors during the conversion process.

This is a known issue and it will be addressed in 'ProWORX 32 version 2.1'. The converter for 'ProWORX 32'
is being completely redesigned.

As a workaround, you can use the attached ProWORX NxT converter to convert the Modsoft program to a
'ProWORX NxT' project which can then be imported into ProWORX 32.

Modosft to NxT Convert.zip

To use the 'ProWORX NxT' converter:

  • Download the attached 'Modsoft to NxT Convert.zip' file and extract all of the files to a temporary
folder on you PC.
  • Open the temporary folder and double click on the file named 'NXTCONV'
  • Select the 'Convert Modsoft database to NxT' option.
  • Browse for the Modsoft source database
  • Specify a new database name for the destination.
  • Click on the 'Start button.



Open 'ProWORX 32' and import the 'ProWORX NxT' database that was created in the step above..