Issue
This resolution was edited on May 23, 2006 to correct the part number from a 140NOE771x0 to a 140NOE77110 only.
Product Line
Quantum
140NOE77110
Resolution
The purpose of this resolution is to inform 140NOE77110 users that the firmware has been upgraded to version 3.5.
A user has the ethernet cable inadvertently disconnected from an NOE77110 while logged in. Attempting to log back in after re-connecting the cable would fail, with the error "User Already Logged In". Firmware v.3.5 now allows the user to re-connect without an error.
Released for:Schneider Electric Global