Issue
The purpose of this resolution is to inform users of Momentum 170LNT71000 Devicenet Communication Adapters of an issue with firmware version 1.21.
Product Line
Momentum
Resolution
If operating for more than 30 seconds after the network becomes active, bidirectional discrete base outputs can freeze at last value when the LNT DeviceNet adapter loses fieldbus communication.
The issue will occur if a Devicenet Comm Adapter version 1.21 is mounted on a bi-directional module and both Polled and Strobed modes are selected at the same time in the Devicenet Scanner IO Parameters.
1) the fieldbus connector is removed from the LNT
2) the head PLC is set from RUN to STOP
3) the fieldbus cable power source is turned off
If the conditions occur within 30 seconds of the fieldbus becoming active, bi-directional module outputs will go to zero.
There is no issue when the LNT is mounted on an output module.
Causes and Fixes
At this time, a workaround to this problem involves selecting only POLLED mode in the Devicenet Scanner when using bi-directional modules.
Devicenet Communication Adapters that have firmware version 1.21 installed are:
-
- 170LNT71000 communication adapters labeled SV 1.21.
- 170LNT71000s labeled SV 1.20 and built after October 2005.
Adapters built before October 2005 labeled SV 1.20, have version v1.20 installed and are not affected by this issue.
This issue is under investigation by Engineering and is expected to be resolved in a firmware update. An update to this Resolution will be available when new information is provided.
Legacy KB System (APS) Data: RESL180245 V1.0, Originally authored by WeDa on 10/27/2006, Last Edited by WeDa on 10/27/2006
Related ranges: Modicon Momentum I/O
Released for:Schneider Electric Global