Issue
The purpose of this Resolution is to specify the copper RTD type used on the STBART0200 module.
Product Line
Advantys STB
STBART0200
Environment
Resolution
The STBART0200 supports copper RTD types, 10 ohms at 0 degrees C.
It does not support copper RTD types, 10 ohms at 25 degrees C.
Released for:Schneider Electric Global