{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
STBACO1210 Loop Current Maximum Load Impedance

Issue
The purpose of this resolution is to inform users of STBACO1210 analog output modules of the Maximum Load Impedance specification.


Product Line
Advantys STB
STBACO1210


Environment


Resolution
The Maximum Load Impedance value defines the maximum impedance allowed in the current loop so currents of 20ma can be provided by the module.

The Maximum Load Impedance specification for the STBACO1210 analog output module is less than or equal to 500 ohms resistive. Load impedance values greater than 500 ohms can prevent the module from producing currents up to 20ma.

Schneider Electric Global