Right click on the section name and choose <properties>. Go to the <condition> tab. Enter a boolean reference or variable which can conditionally disable/enable the section. When this bit is ON, the section is enabled. When this bit is OFF, the section is disabled as indicated by a red mark on the dotted line leading to the section name.
When the bit is Forced ON or OFF, an 'F' is displayed over the red or green dot.
Released for:Schneider Electric Global